Last updated: December 2, 2008
This section is only applicable to EGPRS.
The following topics are discussed in this section:
Setup parameters for this measurement are assumed to be set to their default (Full preset) values unless otherwise stated. This procedure also assumes that the BCH parameter for band is set up correctly for your mobile station and that the appropriate RF IN/OUT Amplitude Offsets have been set to offset loss between the mobile station and the test set.
Operating Mode
(
F1
) and select
Active Cell (EGPRS)
.
Data Conn Type
(
F2
) key, and select
SRB Loopback.
PDTCH Parameters
(
F9
) from the
Call Parms
menu.
Modulation Coding Scheme
(
F11
) from the
PDTCH Parms
menu. The
Modulation Coding Scheme
popup menu appears.
Uplink Modulation Coding Scheme
and select any of the modulation coding schemes.
Close Menu
(
F6
) key.
Turn the mobile on and wait for
Attached
in the
Active Cell:
field.
NOTE |
Start Data Connection
(
F3
) key and watch for the
Active Cell:
field changing to
Transferring
.
EGPRS SRB Bit Error
measurement.The following graphic shows an example of EGPRS SRB Bit Error results. Notice that the number of bits actually tested exceeds the number requested. This occurs because the test set rounds up the number requested to the nearest number that results in an integral number of bursts.
Bit Error Setup
(
F1
) key.
Number of bits to test
. You may also want to set up a
Measurement Timeout
to prevent the measurement from "hanging" if the test set is unable to complete the measurement for any reason.
Close Menu
(
F6
) key.