Last updated: December 2, 2008
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Queries the SRB Loopack bit error measurement. Query returns integrity indicator, bits tested, bit error ratio, and bit error count. |
|
EGPRS TA | ||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:SBERror?" |
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Queries the number of bits that were in error during the last bit error test. See Bit Error Measurement |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:SBERror:COUNt?" |
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Queries the delay (in bursts) that the test set used during the last EGPRS SRB bit error measurement to correlate uplink information bits with downlink information bits. This value is displayed in the Loopback Delay field. This value can be determined automatically, or manually set by the user. See SETup:SBERror:MANual:DELay and SETup:SBERror:LDControl:AUTO . Refer also to the EGPRS SRB Bit Error Measurement for a description of loopback delay and how it is used in the EGPRS SRB bit error measurement. |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:SBERror:DELay?" |
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Queries the intermediate count of bits tested (measurement progress report). See Measurement Progress Report |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
Programming Example OUTPUT 714;"FETCh:SBERror:ICOunt?" |
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Returns the integrity indicator value for the last EGPRS SRB bit error measurement performed. Zero indicates a normal result. See Integrity Indicator for descriptions of non-zero integrity indicators. |
|
EGPRS TA | ||
Range: See Integrity Indicator . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
Programming Example OUTPUT 714;"FETCh:SBERror:INTegrity?" |
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Queries the ratio of bits in error to the number of bits tested during the last EGPRS SRB bit error test and returns it as a percentage. See Bit Error Measurement |
|
EGPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
Programming Example OUTPUT 714;"FETCh:SBERror:RATio?" |