Function
|
GSM TA
|
This command is not applicable to the GSM Test Application. |
GPRS TA |
This command is not applicable to the GPRS Test Application.
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application.
|
GSM/GPRS LA |
Sets the value of the demodulation trigger delay. The demodulation trigger will be delayed by the number of symbols specified with this command.
|
EGPRS LA |
Setting
|
Range: 0 to 200 symbols
Resolution: 1 symbol
|
Query |
Range: 0 to 200 symbols
Resolution: 1 symbol
|
*RST Setting
|
0 |
Requirements |
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above
|
Programming Example:
OUTPUT 714;"CALL:DEModulation:DELay 100"
|