Sets/queries the test set's GPIB address. | ||
GPRS TA | ||
EGPRS TA | ||
14 (this parameter is not affected by any reset operation and can only be changed by direct user access) |
||
Related Topics | Configuring the Test Set's GPIB Address | |
Requirements | ||
OUTPUT 714;"SYSTEM:COMMUNICATE:GPIB:SELF:ADDRESS 14" ! Sets the GPIB address to 14. |
Sets/queries the test set's LAN IP address. The value of A is used to determine the subnet mask, see SYSTem:COMMunicate:LAN[:SELF]:SMASk[:IP4] . If the LAN address is changed the subnet mask should be checked to insure that it is set to the proper class for that LAN address. If the LAN IP address is changed the subnet mask should be checked to insure that it is set to the proper class for that LAN address. (See Configuring the Test Set's LAN )The LAN IP address cannot be changed when CALL:OPERating:MODE is set to CALL. |
||
GPRS TA | ||
EGPRS TA | ||
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B.C. D = 0 to 255 (no embedded spaces). |
||
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B.C.D = 0 to 255 (no embedded spaces). |
||
0.0.0.0 (this parameter is not affected by any reset operation and can only be changed by direct user access) |
||
Related Topics | LAN IP Address | |
Requirements | ||
OUTPUT 714;"SYSTEM:COMMUNICATE:LAN:SELF:ADDRESS '130.015.156.255'" ! Sets the LAN IP address. |
Sets/queries the test set's IPv6 address prefix. See IPv6 Prefix, Upper/Lower (Hex) . |
|
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers.
Double-colon "::" can be used in the IPv6 address as valid. Moreover, "::" can be suffixed at the end of the 19 characters which is also a valid IPv6 address prefix. For example: 2009:1:2:3 and 2009:1:2:3:: are all valid IPv6 address prefixes for the GPIB parameter setting. |
|
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. | |
*RST Setting | "" (Null) |
Requirements | Lab Application Revision: G.00.08 and above |
OUTPUT 714;"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:8960:8960:8960'" !Sets the IPv6 address prefix to 2009:8960:8960:8960. OUTPUT 714;"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:1:2:3'" !Sets the IPv6 address prefix to 2009:1:2:3. OUTPUT 714;"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:1:2:3::'" !Sets the IPv6 address prefix to 2009:1:2:3::. |
GPRS TA | ||
EGPRS TA | ||
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B.C. D = 0 to 255 (no embedded spaces). |
||
Range: 15 characters formatted as follows: A.B.C.D. The range of values for A= 0 to 126 and 128 to 223. The range of values for B.C.D = 0 to 255 (no embedded spaces). |
||
0.0.0.0 (this parameter is not affected by any reset operation and can only be changed by direct user access) |
||
Related Topics | LAN 2 PORT | |
Requirements | ||
OUTPUT 714;"SYSTEM:COMMUNICATE:LAN:SELF:ADDRESS2 '130.015.156.255'" ! Sets the LAN 2 IP address. |
Sets/queries the test set's IPv6 Default Router Interface ID. See IPv6 Default Router Interface ID, Upper/Lower (Hex) for details. |
|
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers. Double-colon "::" can be used in the IPv6 Default Router Interface ID as valid. Moreover, "::" can be prefixed at the beginning of the 19 characters which is also a valid IPv6 Default Router Interface ID. For example: 8960::1, ::1:2 and 8960:8960:146.208.232:220 are all valid IPv6 Default Router Interface IDs for the GPIB parameter setting. The IPv6 Default Router Interface parameter is also IPv4 address-compatible with the format: ::W.X.Y.Z, where W.X.Y.Z is the dotted decimal representation of an IPv4 address. For example, ::8960:8960:146.208.232:220 and 8960:8960:146.208.232:220 are all valid IPv6 Default Router Interface IDs for the GPIB parameter setting. |
|
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. | |
*RST Setting | "" (Null) |
Requirements | Lab Application Revision: G.00.08 and above |
OUTPUT 714;" SYSTem:COMMunicate:LAN:DGATeway:IP6:IID '0000:0000:821D:B001'" !Sets the test set's IPv6 Default Router Interface ID to 0000:0000:821D:B001. |