Broadcast Channel (BCCH) Update Procedure (SIB Contents)

Broadcast Channel (BCCH) Update Procedure (SIB Contents)

Last updated: January 15, 2009

While in active cell operating mode, the test set broadcasts the System Information Message on the BCCH. The System Information Message consists of a Master Information Block (MIB) and several System Information Blocks (SIBs 1, 2, 3, 5, 7 and 11). The information in these SIBs helps the UE (mobile station) successfully communicate with the network.

The user-settable parameters contained in the MIB and SIBs are listed in the table below. When you change any of these parameters, the test set changes the information it sends on the BCCH accordingly. Some of these parameters can not be changed while in active cell operating mode (you must first switch to cell off operating mode). Changing any of the other parameters causes the test set to perform a BCCH update procedure if the call status is idle and BCCH Update Page is set to Auto (if the test set is on a connection with a UE, the test set will post an error if you try to change any of these parameters). During a BCCH update procedure, the test set sends a Paging Type I message to the UE indicating that it needs to re-read the BCCH. If your UE does not support the BCCH update procedure, you may set BCCH Update Page to Inhibit , which prevents the test set from sending a Paging Type I message to the UE (the test set still updates the BCCH). However, note that the UE will then be unaware of the changes in the BCCH. See BCCH Update Page for more information.

BCCH Settable Parameters
Change Prompts BCCH Update?
MIB Settable Parameters:
Mobile Country Code (MCC) Yes
Mobile Network Code (MNC) Yes
  
SIB 1 Settable Parameters:
ATT (IMSI Attach) Flag State Yes
DRX Cycle Length (CN Domain) Yes
Local Area Code (LAC) Yes
N313 Successive Out-Of-Sync Reception Max Yes
N315 Successive In-Sync Reception Counter Yes

Network Mode of Operation

Yes
PS Domain Information Yes
Routing Area Code (RAC) Yes
T313 Out-Of-Sync Reception Timer Yes

T3212 Periodic Location Update Timer ( lab application only )

Yes

  

SIB 3 Settable Parameters:

Cell Barred State ( lab application only ) Yes
Cell Barred Timer (Tbarred) ( lab application only ) Yes
Cell Identity Yes
Hysteresis 1 (Qhyst1) ( lab application only ) Yes
Hysteresis 2 (Qhyst2) ( lab application only ) Yes
Intra-frequency Cell Reselection Indicator ( lab application only ) Yes
Maximum Uplink Transmit Power Level Yes
Minimum Required Quality Level (Qqualmin) ( lab application only ) Yes
Minimum Required Rx Level (Qrxlevmin) ( lab application only ) Yes
Quality Measure ( lab application only ) Yes
Sintersearch ( lab application only ) Yes
Sintrasearch ( lab application only ) Yes
Timer (Treselection) ( lab application only ) Yes
  

SIB 5 Settable Parameters:

Note, the Transmit SIB5bis setting determines whether SIB5 or SIB5bis is transmitted by the test set. Changing Transmit SIB5bis causes a BCCH update.

AICH Channelization Code No (this setting can not be changed in active cell operating mode)
AICH Level No (this setting can not be changed in active cell operating mode)
Available Subchannels (Bit Mask) Yes
Constant Value Yes
E-DCH Cell Indicator (lab application or feature-licensed test application only) Yes
Frequency Band Indicator and Frequency Band Indicator 2 (see Frequency Band Indicator State ). No (this setting can not be changed in active cell operating mode)
HSDPA Cell Indicator (lab application or feature-licensed test application only) Yes
Manual PRACH Bc Yes
Manual PRACH Bd Yes
PICH Channelization Code No (this setting can not be changed in active cell operating mode)
PICH Level No (this setting can not be changed in active cell operating mode)
PRACH Bc/Bd Control Yes
PRACH Power Ramp Step Yes
PRACH Preambles Yes
PRACH Ramping Cycles (MMAX) Yes
PRACH Scrambling Codeword No (this setting can not be changed in active cell operating mode)
PRACH Signature Yes
Primary CPICH TX Power Yes
S-CCPCH Channelization Code No (this setting can not be changed in active cell operating mode)
  
SIB 7 Settable Parameters:
Uplink Interference Yes
  
SIB 11 Settable Parameters:
Cell Info List Yes
GSM <num> Cell BCC Yes
GSM <num> Cell BCH ARFCN Yes
GSM <num> Cell Cell Reselection Min Rx Level ( lab application only ) Yes
GSM <num> Cell NCC Yes
GSM <num> Cell Shared ARFCN Indicator Yes
GSM <num> Cell State Yes
Inter-freq <num> Cell Cell Reselection Offset1 ( lab application only ) Yes
Inter-freq <num> Cell Cell Reselection Offset2 ( lab application only ) Yes
Inter-freq <num> Cell DL Channel Yes
Inter-freq <num> Cell Scrambling Code Yes
Inter-freq <num> Cell State Yes
Intra-freq <num> Cell Cell Reselection Offset1 ( lab application only ) Yes
Intra-freq <num> Cell Cell Reselection Offset2 ( lab application only ) Yes
Intra-freq <num> Cell Scrambling Code Yes
Intra-freq <num> Cell State Yes
Quality Measure ( lab application only ) Yes

Related Topics


How Do I Change Cell Parameters?

How Do I Change the SIB11 Cell Info List?

How Do I Change Uplink Parameters?

SIB11 Cell Info List