Cell Information

 Last updated: April 27, 2013

 

 Reselection Parameters

 This section is only applicable to the lab application.

 These settings can only be changed when call status is Idle . If BCCH Update Page is set to Auto and you change these settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure (SIB Contents) . If BCCH Update Page is set to Inhibit (the default value) and you change these settings while your UE is camped to the test set, you must force your UE to re-read the BCCH to observe the change (see BCCH Update Page for more details).

 

 Access Restriction Parameters

 This section is only applicable to the lab application.

 These settings can only be changed when call status is Idle . If BCCH Update Page is set to Auto and you change these settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure (SIB Contents) . If BCCH Update Page is set to Inhibit (the default value) and you change these settings while your UE is camped to the test set, you must force your UE to re-read the BCCH to observe the change (see BCCH Update Page for more details).

 These parameters are sent in the Cell Access Restriction information element on SIB3. See 3GPP TS 25.331 s10.3.2.1.

 

 UE Timer and Constant Parameters

 The following settings, with the exception of the T3312 Periodic RA Update Timer and T3312 Periodic RA Update Units settings, can only be changed when call status is Idle . If BCCH Update Page is set to Auto and you change these settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure (SIB Contents) . If BCCH Update Page is set to Inhibit (the default value) and you change these settings while your UE is camped to the test set, you must force your UE to re-read the BCCH to observe the change (see BCCH Update Page for more details).

 

Related Topics


 

How Do I Change Cell Info?

 Two-Cell Test System

 Broadcast Channel (BCCH) Update Procedure (SIB Contents)

 Cell Parameters