Programming a Block Error Ratio Measurement

Programming a Block Error Ratio Measurement

Last updated: January 16, 2009

  1. Set MS Loopback Type to Type 2 using the CALL:MS:LOOPback:TYPE command.
  2. Set Uplink DTCH RMC CRC Presence to Used for Data using the CALL:SERVice:RBTest:DTCHannel:CRC[:PRESence] command.
  3. Prompt the user to power the UE on and wait for it to camp to the test set, then continue the program.
  4. Set Paging Service to RB Test Mode using the CALL:PAGing:SERVice[:TYPE] command.
  5. Set Channel Type to 12.2k RMC using the CALL:SERVice:RBTest:RAB command.
  6. Originate a call using the CALL:ORIGinate[:AUTO] command.
  7. Set Cell Power as needed using the CALL[:CELL]:POWer[:SAMPLitude][:SELected] command.
  8. Set up the measurement using the SETup:WBLerror commands.
  9. INITiate the measurement using the INITiate command.
  10. FETCh the measurement results using the FETCh:WBLerror commands.

Related Topics


Block Error Ratio (BLER) Measurement Description

Step 4: Make a Connection