Block Error Ratio (BLER) Measurement Description

Last updated: February 28, 2014

How is a Block Error Ratio Measurement Made?

3GPP TS 34.121, F.6.1.1 defines block error ratio (BLER) as follows: "A Block Error Ratio is defined as the ratio of the number of erroneous blocks received to the total number of blocks sent. An erroneous block is defined as a Transport Block, the cyclic redundancy check (CRC) of which is wrong."

To perform a block error ratio measurement, you must be on a Radio Bearer Test Mode call. The block error ratio measurement can be performed for both Symmetrical RMCs and Asymmetrical RMCs . For RMCs with a downlink rate of 12.2, 64 or 144 kbps, the test set sends a block every 20 ms. For RMCs with a downlink rate of 384 kbps, the test set sends a block every 10 ms.

The data sent on the downlink is determined by the DL DTCH Data setting.

Symmetrical RMCs

For Symmetrical RMCs (which use Transparent Mode (TM) RLC entities on the DTCH), the test set measures block error ratio by sending data and CRC bits in the downlink transport blocks to a UE that is configured in loopback mode 2 (UE Loopback Type must be set to Type 2 ). The UE then loops the data bits and CRC bits from the downlink transport blocks into the uplink transport blocks and transmits them in the uplink. The test set then generates a CRC from the data bits received in the uplink transport block and compares this calculated CRC against the CRC received in the uplink transport block (this CRC is the downlink CRC for the downlink transport block, looped back up by the UE). If the CRCs do not match, the transport block is defined to be a "block error."

To perform the block error ratio measurement for symmetrical RMCs, Uplink DTCH RMC CRC Presence must be set to Used for Data . This disables the uplink CRC, to allow room for the UE to loop back the downlink CRC for each block (there are an equal number of available bits in the uplink and downlink, if the UE were to transmit an uplink CRC, it would not be able to loop back the downlink CRC).

Asymmetrical RMCs

For Asymmetrical RMCs (which use Acknowledged Mode (AM) RLC entities on the DTCH), the test set increments the Block Error Count when it receives a retransmission request from the UE. (The UE generates a CRC from the data bits received in the downlink transport block, and compares this calculated CRC against the CRC received in the downlink transport block. If the CRCs do not match, the UE sends a retransmission request to the test set.)

UE Control During FDD Test Mode Operation

The FDD Test Operating Mode does not provide radio bearer setup control of the UE for test mode operation. You must configure the UE in loopback mode 2 and synchronize it to the test set's downlink signal in order to make this measurement in FDD test operating mode.

The uplink transport format must include both the DTCH and the DCCH; however, only the DTCH information is used for the block error ratio measurement.

Note that Asymmetrical RMCs are not available in FDD test operating mode.

Block Error Ratio Measurement Parameters

The trigger source for this measurement is always protocol-based (see Trigger Source Description ).

Block Error Ratio Measurement Results

Block Error Ratio Input Signal Requirements

Related Topics


Manual Operation: How Do I Make a Block Error Ratio (BLER) Measurement?

Programming a Block Error Ratio Measurement

Block Error Ratio Troubleshooting

HSDPA Block Error Ratio Measurement Description

Loopback Bit Error Ratio (BER) Measurement Description

What 3GPP W-CDMA/HSPA Conformance Tests Are Supported?