Using Standard Setups/Presets)
Selected (SeeEVM) calculations.
, when selected, includes synchronization and pilot symbols in Error Vector Magnitude (Synchronization and pilot symbols have magnitude "1" and appear on the sync/pilot locus of the constellation diagram at phase angles that correspond to the standards.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |