Multiple PDP Contexts Information

Last updated: November 6, 2013

This section is only applicable to the lab application.

The topics discussed in this section are:

Multiple PDP Contexts Overview

The Multiple PDP Contexts functionality allows you to test the UEs running simultaneous PS services, for example, to test the UE that is sending/receiving emails while performing video stream. There are two categories for multiple PDP contexts:

The test set supports to setup multiple (up to two) primary PDP contexts simultaneously with the UE. You can enable/disable the primary PDP contexts independently from one another, with each PDP context using its own IP address (either IPv4 or IPv6) and QOS profile, see Multiple PDP Contexts Parameters .

Operating Considerations

Multiple PDP Contexts Setup

You can set two DUT IP addresses to support at most two primary PDP contexts, see DUT IP Setup . The actual DUT IP address used (can be an IPv4 address or an IPv6 address) for each PDP connection is according to the UE's requests and your DUT IP settings.

Multiple PDP Contexts Parameters

  • First primary PDP Context QoS profile

    This setting allows you to configure the QoS parameters for the first primary PDP context if the first DUT IP is configured. If it is configured to QoS Profile 1 or QoS Profile 2 , the requested QoS from UE will be ignored and the QoS will be configured based on the associatedQoS Profile1/2 Setup . If it is configured to None and the UE requested QOS parameters are valid, the test set will use the requested QoS, otherwise the test set will use the default value(s) in the accept message.

    GPIB Command: CALL:MS:IP:ADDRess[1]:CONText:PRIMary:QOService

  • Second primary PDP Context QoS profile

    This setting allows the user to configure the QoS parameters for the second primary PDP context if the second DUT IP is configured. If it is configured to QoS Profile 1 or QoS Profile 2 , the requested QoS from UE will be ignored and the QoS will be configured based on the associatedQoS Profile1/2 Setup . If it is configured to None and the UE requested QOS parameters are valid, the test set will use the requested QoS, otherwise the test set will use the default value(s) in the accept message.

    GPIB Command: CALL:MS:IP:ADDRess2:CONText:PRIMary:QOService

You are not allowed to change these settings while in Active Cell operating mode and the data status is other than Idle .

QoS Profile1/2 Setup

For either the first or the second primary PDP context, if its QOS profile is set to QoS Profile 1 or QoS Profile 2 (see Multiple PDP Contexts Parameters ), the requested QoS from UE will be ignored and the IE Negotiated QoS fields of ACTIVATE PDP CONTEXT ACCEPT message for this PDP connection will be configured based on the following settings:

These settings can only be changed while the data status is Idle .

Related Topics

CALL:MS:IP:ADDRess