Last updated: December 3, 2008
GSM TA | ||
This query returns the bit error measurement results. The integrity indicator, bits tested, bit error ratio, and bit error count are returned. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
This query returns the total number of information bits tested during the last bit error measurement. See FETCh:GBERror:COUNt? . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
This query returns the CRC (Frame Check Sequence) Error Count found during the last GBER measurement. Each block that fails its CRC will cause the CRC Error Count result to increment. The CRC Error Count affects the BLER measurement results differently depending on the GBER Bad Block Handling setting. For more information on the GBER Bad Block Handling setting see SETup:GBERror:BBLocks . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
This query returns the count of erroneous bits found during the last bit error measurement. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
This query returns the block delay the test set used during the last bit error measurement. This value can be determined automatically by the test set, or you can set it manually. See SETup:GBERror:MANual:DELay and SETup:GBERror:LDControl:AUTO for setting this value manually. Refer also to the GPRS Bit Error Measurement for a description of block delay and how it is used in the bit error measurement. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision A.03: Upper limit on range changed from 6 to 12 |
GSM/GPRS/ EGPRS LA |
Revision C.03: Upper limit on range changed from 6 to 12 |
GSM TA | ||
Queries the intermediate count (measurement progress report) of bits tested. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
This query returns the integrity indicator value for the last bit error measurement performed. Zero indicates a normal result. See Integrity Indicator for descriptions of non-zero integrity indicators. |
||
Range: See Integrity Indicator . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | ||
This query returns the ratio of erroneous bits found during the last bit error measurement. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |