Last updated: December 4, 2008
This command is not applicable to the GSM TA. | |||
This command sets/queries the setting for the GBER Bad Block Handling parameter. The GBER Bad Block Handling parameter controls how the bad blocks are used while calculating the BER. This command as three options:
|
|||
Setting | |||
*RST Setting | |||
Requirements |
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | |||
OUTPUT 714;"SETup:GBERor:BBLocks EXClude" ! Sets GBER measurement to exclude all bits within a bad block while calculating the BER. |
This command sets/queries the loopback delay control mode. If loopback delay control mode is automatic (ON), the test set determines the block delay value that allows the correlation between uplink and downlink data. While the loopback delay control is automatic, the test set attempts to determine the loopback delay in the following cases:
If loopback delay control mode is manual (OFF), the test set uses the block delay you specify using SETup:GBERror:MANual:DELay . Refer to How is a GPRS Bit Error (GBER) Measurement Made? for a description of block delay and its use in the BER measurement. |
||
Setting | ||
*RST Setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:GBERror:LDControl:AUTO OFF" ! Sets the loopback delay control mode to manual. |
This command sets/queries the block delay when loopback delay control mode is manual. To set the delay mode to manual, refer to SETup:GBERror:LDControl:AUTO . Refer to GPRS Bit Error Measurement for a description of block delay and how it is used in this measurement. |
||
Setting | ||
*RST Setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:GBERror:MANual:DELay 6" ! Sets the number of blocks to 6. |
THIS COMMAND IS OBSOLETE. Please use
SETup:GBERror:BBLocks
instead.
This command sets/queries the zero bad blocks state for BER measurements. The zero bad blocks state determines how a bad block is interpreted. A block is defined as bad if either:
When set to On, all bits within a bad block are set to zero. This results in an average error rate of 50%. Setting this command to On is equivalent to setting the SETup:GBERror:BBLocks to Zero. When set to Off, the value of bits within a bad block are not altered before being measured. This lowers the overall BER value measured. Setting this command to Off is equivalent to setting SETup:GBERror:BBLocks to INClude. |
||
Setting | ||
*RST Setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:GBERror:ZBBLocks:STATe OFF" ! Sets the zero bad blocks state to off. |