Last updated: December 3, 2008
This query returns the integrity indicator and a comma separated list containing the measured average audio levels for each of the 20 audio tones that are turned on. The query returns NAN (9.91E+37) for any audio tone that is turned off. See SETup:MTAudio:GENerator:LEVel:DOWNlink:ALL[:SAMPlitude] for more information on turning audio tones off and on |
||
GSM/GPRS LA | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns the average multi-tone audio distortion measurement result for audio tone 1. The SINAD/Distortion state must be on for this result to be returned. See SETup:MTAudio:SDIStortion:STATe . |
||
GSM/GPRS LA | ||
EGPRS TA | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns the average frequency measurement result for audio tone 1. The SINAD/Distortion state must be on for this result to be returned. See SETup:MTAudio:SDIStortion:STATe . |
||
GSM/GPRS LA | ||
EGPRS TA | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns the intermediate count of multi-tone audio multi-measurements completed. This value is not available over the manual interface. |
||
EGPRS TA | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns the integrity indicator for the last multi-tone audio measurement completed. Zero indicates a normal measurement. See Integrity Indicator for descriptions of non-zero integrity indicators. | ||
EGPRS TA | ||
Range: See
Integrity Indicator
. |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns a comma separated list containing the measured average audio levels for each of the 20 audio tones that are turned on. The query returns NAN (9.91E+37) for any audio tone that is turned off. See SETup:MTAudio:GENerator:LEVel:DOWNlink:ALL[:SAMPlitude] for more information on turning audio tones off and on. | ||
EGPRS TA | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns information about whether the multi-tone audio level measurement results exceeded the mask limits. | ||
EGPRS TA | ||
0: Passed 1: Failed 9.91E+37 (NAN): results can not be determined |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns the average SINAD measurement for audio tone 1. The SINAD/Distortion state must be on for this result to be returned. See SETup:MTAudio:SDIStortion:STATe . |
||
EGPRS TA | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |
This query returns the total average measured audio level. The value is returned in units of Vrms when the measurement mode is downlink and in percentage (%) when the measurement mode is uplink. (See SETup:MTAudio:MEASurement:MODE .) When the SINAD/Distortion state is on, this result is the average audio level of audio tone 1. See SETup:MTAudio:SDIStortion:STATe . |
||
EGPRS TA | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA |