Occupied Bandwidth (OBW) Measurement

Last updated: 2014-11-28

Occupied Bandwidth (OBW) Measurement Description

Occupied Bandwidth (OBW) Measurement Parameters

Occupied Bandwidth (OBW) Measurement Results

Input Signal Requirements

Occupied Bandwidth (OBW) Measurement Description

As defined by 3GPP TS 34.122 Section 5.5.1, Occupied Bandwidth (OBW) measurement is a measure of the bandwidth containing 99 % of the total integrated power for transmitted spectrum and is centered on the assigned channel frequency. The test set allows the percentage of total integrated power to be adjusted from 70.0 to 99.0%.

According to the standard, the occupied channel bandwidth shall be less than 1.6 MHz.

This measurement requires the calibration data of the measurement receiver path gain, which are part of the results of the measurement calibration, see Calibrate Measurements.

Occupied Bandwidth (OBW) Measurement Parameters

Occupied Bandwidth (OBW) Measurement Results

Input Signal Requirements

Related Topics

GPIB Commands: SETup:TOBWidth, FETCh:TOBWidth