Compressed Mode

Compressed Mode

Last updated: October 19, 2012

This section is only applicable to the lab application.

Compressed Mode Overview

Compressed mode places gaps in the downlink and uplink transmissions that allow a UE, while on a call, to perform measurements on neighboring cells of a different frequency than its current serving cell. The UE can perform measurements on neighboring GSM, W-CDMA or E-UTRAN cells.

The network specifies the transmission gap pattern sequences (TGPSs), which control when the transmission gaps occur and their duration. During radio frames that contain transmission gaps, the UE and network use a lower spreading factor to avoid losing any data due to the smaller transmit/receive window caused by the transmission gap.

The compressed mode feature allows you to specify up to 4 TGPSs, each with a different measurement purpose, if desired. Each TGPS consists of repetitions of one transmission gap pattern, which can include one or two transmission gaps.

The test set supports compressed mode by spreading factor reduction in both the downlink and uplink. Note, however, that the test set does not transmit downlink compressed frames at an increased power level; compressed frames are transmitted at the same power level as non-compressed frames - the power level determined by the Cell Power setting. Additionally, the test set's DPCH is not turned off during the transmission gaps. The test set supports compressed mode on the following connection types and channel configurations: RB Test Mode, HSDPA RB Test Mode, HSUPA RB Test Mode, AMR voice, CS Data/Video Call, PS Data, HSDPA PS Data and HSUPA PS Data. The 384k RMC is not supported as it is not compressible by spread factor reduction because the uplink 384k DPCH already uses the minimum DPCH spreading factor of 4 (3GPP TS 25.212 s4.4.3.2 states, "The spreading factor (SF) can be reduced by 2 during one compressed radio frame to enable the transmission of the information bits in the remaining time slots of the compressed frame. This method is not supported for SF=4.").

The test set supports compressed mode for 384k downlink channels. Note that the test set does not support compressed mode for the 384k RMC, 384k UL/384k DL PS or 384k UL/HSDPA DL PS channels. These channels are not compressible by spread factor reduction because the uplink 384k DPCH already uses the minimum DPCH spreading factor of 4.

A consequence of the SF/2 spreading factor reduction method is that during compressed frames, the DPCH takes up twice as much code channel space as in non-compressed frames. As the downlink channels have to share the same code space care must be taken to ensure that compressed frames do not collide with other connected mode channels (for example, OCNS).

The test set uses an arbitrary channelization code allocation with collision detection scheme. The test set does not block any operations that cause code collision (such as the operation to activate Compressed Mode) but instead permits collisions.

However, when the test set has detected that a collision has occured, a persistent error message is generated,and since the UEs behaviour is unpredictable, any measurement results provided by the test set will not be reliable.

To avoid the possibility of collision, it is recommended that you use the test set's Downlink Channel Code Preset Configurations before enabling compressed mode. For example, a preset configuration is provided for Compressed Mode with 384k DL DPCH (Non-HSDPA) . You may also find it useful to refer to 3GPP TS 34.121 Annex E.6 "Downlink Physical Channels Code Allocation".

The following table summarizes the vaild channel code ranges that are available for use in compressed mode according to the specifications. See Downlink Channel Codes for additional information about channelization codes.

Channel Types Supported in Compressed Mode and Channelization Code Range
Channel Type Valid Compressed Mode Channelization Code Range Lab Application Front Panel Setting
5.9k - 4.75k AMR Voice 2 to 255
(The following codes will avoid the possibility of a collision: 12, 13, 20, 21, 40, 43, 58, 126, 127, 142, 153, 174, 235, 255)
DPCH 15 ksps (OVSF 256) Channelization Code
12.2k RMC
33k No Coding RMC
12.2k - 6.7k AMR Voice
14.4k UL/14.4k DL CS Data RAB
1 to 127
(The following codes will avoid the possibility of a collision: 20, 29, 37, 45, 60, 70, 76, 87, 93. Please note that the default value of 9 is not valid.)
DPCH 30 ksps (OVSF 128) Channelization Code
12.2k RMC + HSDPA 1 to 127
(The following codes will avoid the possibility of a collision: 20, 29, 37, 45, 54)
HSDPA DPCH 30 ksps (OVSF 128) Channelization Code
64k/HSDPA PS (3.4k SRB used while on an HSDPA packet data connection)
128k UL/HSDPA DL PS (3.4k SRB used while on an HSDPA packet data connection)
2 to 255
(The following codes will avoid the possibility of a collision: 40, 43, 58)
HSDPA DPCH 15 ksps (OVSF 256) Channelization Code,
64k RMC
12.2k UL/64k DL AM RMC
57.6k UL/57.6k DL CS Data RAB
64k UL/64k DL CS Data RAB
64k UL/64k DL PS Data RAB
1 to 31
(The following codes will avoid the possibility of a collision: 24, 25, 26, 27)
DPCH 120 ksps (OVSF 32) Channelization Code
144k RMC
12.2k UL/144k DL AM RMC
1 to 15
(The following codes will avoid the possibility of a collision: 12, 13)
DPCH 240 ksps (OVSF 16) Channelization Code
12.2k UL/384k DL AM RMC
64k UL/384k DL AM RMC
64k UL/384k DL RMC
64k UL/384k DL PS
128k UL/384k DL PS
6

DPCH 480 ksps (OVSF 8) Channelization Code

See Current Service Type for more information about the various channel types available in the test set.

Enabling/Disabling Compressed Mode

Once on a connection, you may enable (or disable) compressed mode operation by selecting Enable Compressed Mode (or Disable Compressed Mode ) or using the CALL:COMPressed:ENABle command. Upon successful activation of compressed mode, the Overall CM state changes to On in the Compressed Mode TGPS Information window, and any active TGPSs are displayed as On .

The Call Setup Screen also displays Compressed Mode State (which corresponds to Overall CM ) under Call Processing Status . Compressed Mode State/Overall CM can be queried using the CALL:STATus:COMPressed:STATe? command. If one or more TGPSs is active, Compressed Mode State/Overall CM is displayed as On . You can query which TGPSs are active using the CALL:STATus:COMPressed:TGPSequence:ALL:STATe? command. Note that if <num> TG Pattern Repetition Count (TGPRC) is non-zero, when the specified number of transmission gap pattern repetitions have occurred, the state of that TGPS changes from On to Off .

The message that activates compressed mode specifies a starting time that gives the UE sufficient time to respond with the proper messaging before compressed mode is enabled. If the proper messaging is received, Compressed Mode State/Overall CM changes to On .

You are not allowed to enable/disable compressed mode while Dual Cell HSDPA is configured.

Shared Compressed Mode Parameters

TGPS Parameters

As per 3GPP TS 25.215 s6.1.1.2, "A transmission gap pattern sequence consists of consecutive occurrences of transmission gap pattern 1, where transmission gap pattern 1 consists of one or two transmission gaps."

If TGPS Definition During Call Setup is set to Off , the following parameters can only be changed when compressed mode is not active. If TGPS Definition During Call Setup is set to RB Setup , the following parameters can only be changed when the connection status is idle.

The following parameters, (described in 3GPP TS 25.215 s6.1.1.2), characterize the transmission gap pattern:

The following parameters, (described in 3GPP TS 25.215 s6.1.1.2), control the transmission gap pattern sequence start and repetition:

In addition to the parameters described above, for downlink power control in compressed mode, the target SIR needs to be changed in several frames. The four values DeltaSIR1, DeltaSIRafter1, DeltaSIR2 and DeltaSIRafter2 are signalled by the test set to the UE (3GPP TS 25.331 s10.3.6.33). DeltaSIR2 and DeltaSIRafter2 are not transmitted by the test set.

The following figure shows two sample TGPSs and the resulting compressed mode UE waveform as measured by the phase discontinuity measurement (see How Do I Make a Phase Discontinuity Measurement? ).

Key Considerations when Specifying the Transmission Gap Pattern Sequences

UE Measurement Setup

When you enable compressed mode, the UE compresses its output according to the transmission gap pattern information it has been given by the test set (in the RB Setup or Physical Channel Reconfiguration message, as determined by the TGPS Definition During Call Setup setting). However, the UE will not send any Measurement Reports to the test set unless UE Measurements in Compressed Mode is set to On when compressed mode is enabled (the UE Measurements in Compressed Mode setting determines whether compressed mode is activated using a Measurement Control message, which orders the UE to return Measurement Reports, or using a Physical Channel Reconfiguration message, which does not request Measurement Reports).

The following table summarizes the options for enabling compressed mode and UE measurements:

Summary of Options for Enabling Compressed Mode and UE Measurements
TGPS Definition During Call Setup UE Measurements in Compressed Mode TGPS Definition occurs in which message? TGPS Activation occurs in which message? Result
RB Setup Off RB Setup message Physical Channel Reconfiguration message TGPS definition occurs during call setup, compressed mode is activated without UE measurements.
Off Off Physical Channel Reconfiguration message Physical Channel Reconfiguration message TGPS definition occurs after the call is established, compressed mode is activated without UE measurements.
RB Setup On RB Setup message Measurement Control message TGPS definition occurs during call setup, compressed mode is activated with UE measurements.
Off On Physical Channel Reconfiguration message Measurement Control message TGPS definition occurs after the call is established, compressed mode is activated with UE measurements.

See Compressed Mode Ladder Diagrams for more information about the messages exchanged during these operations.

To receive measurement results from the UE, as mentioned above you must set UE Measurements in Compressed Mode to On , but you must also ensure that the Measurement Configuration setting matches the <num> TG Measurement Purpose (TGMP) for at least one active TGPS.

When you enable compressed mode with UE measurements, the test set sends a Measurement Control message to the UE which includes a list of cells to measure (the SIB11 cell info list for inter-frequency cells or for GSM cells, or SIB19 cell info list for E-UTRAN cells, depending upon the Measurement Configuration setting). Thus, before enabling compressed mode with UE measurements, ensure that the cells in the SIB11 for SIB19 cell info lists are in a frequency band that is supported by your UE.

As the UE returns Measurement Reports, the results are posted to the front panel and available via GPIB (see Compressed Mode UE Reported Measurements ).

The UE performs periodic measurements on the neighbor cells that you specify. You may configure how many measurements are reported, and how often, using the following parameters:

Compressed Mode Preset Configurations

From the front panel only, you can select the following preset configurations for compressed mode to quickly configure the test set for one of eight typical compressed mode measurement scenarios.

Compressed Mode Preset Configurations
Setting Compressed Mode Preset Configuration for Inter-freq FDD and Inter-RAT GSM Measurements
Inter-freq FDD Meas Inter-RAT Meas
(GSM - Carrier RSSI)
Inter-RAT Meas
(GSM - Init BSIC ID)
Inter-RAT Meas
(GSM - BSIC Reconfirm)
Inter-RAT GSM Meas

Inter-freq FDD &
Inter-RAT GSM Meas

3GPP reference TS 34.121 Table C.5.2 Set 1 TS 34.108 Table 6.8.6, TS 34.121 Table C.5.2 Set 2 TS 34.108 Table 6.8.6 TS 34.108 Table 6.8.6 TS 34.108 Table 6.8.6 TS 34.108 Table 6.8.7
TGPS State 1,0,0,0 1,0,0,0 1,0,0,0 1,0,0,0 1,1,1,0 1,1,1,1
Meas Purpose FDDM,GSMR,
GIBI,GBR
GSMR,GIBI,
GBR,FDDM
GIBI,GSMR,
GBR,FDDM
GBR,GIBI,
GSMR,FDDM
GBR,GSMR,
GIBI,FDDM
FDDM,GSMR,
GBR,GIBI

UE Meas in Comp Mode

On On On On On On
Meas Config Inter-freq Inter-RAT Inter-RAT Inter-RAT Inter-RAT Inter-RAT (to perform inter-freq measurements you must disable comp mode, change this setting to inter-freq, then enable comp mode)
TGPRC 0,0,0,0 0,0,0,0 0,0,0,0 0,0,0,0 0,0,0,0 0,0,0,0
TGCFN 0,4,15,18 0,4,15,18 0,4,15,18 0,4,15,18 0,2,4,8 0,4,15,18
TGSN 4,4,4,4 4,4,4,4 4,4,4,4 4,4,4,4 4,4,4,4 8,8,8,8
TGL1 7,7,7,7 7,7,7,7 7,7,7,7 7,7,7,7 7,7,7,7 14,14,14,14
TGL2 0,0,0,0 0,0,0,0 0,0,0,0 0,0,0,0 0,0,0,0 0,14,0,14
TGD 270,270,
270,270
270,270,
270,270
270,270,
270,270
270,270,
270,270
270,270,
270,270
270,60,
270,45
TGPL 3,8,8,8 12,8,8,8 8,8,8,8 8,8,8,8 8,12,8,8 12,24,24,24

Downlink Frame Structure Type

Type A Type A Type A Type A Type A Type A
Compressed Mode Preset Configurations
Setting Compressed Mode Preset Configuration for Inter-RAT E-UTRA Measurements
Inter-RAT Meas (E-UTRA FDD-RSRP)

Inter-RAT Meas (E-UTRA FDD-RSRQ)

3GPP reference
TGPS State 1,0,0,0 1,0,0,0
Meas Purpose EUTR, GSMR, GBR, GIBI EUTR, GSMR, GBR, GIBI
E-UTRA Meas Quantity RSRP RSRQ

UE Meas in Comp Mode

On On

Meas Config

Inter-RAT EUTRA Inter-RAT EUTRA
TGPRC 0,0,0,0 0,0,0,0
TGCFN 0,10,15,25 0,10,15,25
TGSN 10,10,10,10 10,10,10,10
TGL1 10,10,10,10 10,10,10,10
TGL2 0,0,0,0 0,0,0,0
TGD 270,270,270,270 270,270,270,270
TGPL 8,8,8,8 8,8,8,8

Downlink Frame Structure Type

Type A Type A

Additional Considerations While in Compressed Mode Operation

Compressed Mode Operation While in FDD Test Operating Mode

In FDD Test Operating Mode , you can configure up to 4 TGPSs using the TGPS Parameters (except TGMP and TGCFN) or the Compressed Mode Preset Configurations . Note that when you enable compressed mode in FDD test operating mode, the test set does not order the UE to enter compressed mode. Rather, enabling compressed mode simply causes the test set to start compressing its downlink DPCH according to the TGPSs you've specified and to expect the same compressed mode pattern(s) in the uplink DPCH. Before enabling compressed mode operation, you must synchronize your UE to the test set's signal and configure the UE's compressed mode transmission to match the TGPSs you've specified in the test set. Then, when you enable compressed mode in the test set you must also order your UE to begin compressing its signal on the <num> TG Starting CFN frame.

The <num> TG Relative CFN (TGCFN) settings are not applicable to FDD test operating mode. You must use the <num> TG Starting CFN settings to specify when compressed mode operation begins, and ensure that your UE is set to begin compressed mode operation at the CFN that matches this setting.

Because there is no signaling in FDD test operating mode, the UE can not perform neighbor cell measurements during compressed mode (the test set can not send a Measurement Control message to the UE to start neighbor cell measurements). Thus, the <num> TG Measurement Purpose (TGMP) settings are not applicable to FDD test operating mode.

The following settings are only available in FDD test operating mode.

Related Topics


Manual Operation: How Do I Enable Compressed Mode and Obtain UE Measurement Results?

Compressed Mode UE Reported Measurements

Compressed Mode Ladder Diagrams

Troubleshooting Compressed Mode Operation

CALL:COMPressed

CALL:STATus

CALL:FDDTest

SIB11 Cell Info List

SIB19 E-UTRA Info List