How Do I Make a Block Error Ratio (BLER) Measurement?

How Do I Make a Block Error Ratio (BLER) Measurement?

Last updated: January 15, 2009

Measuring Block Error Ratio

  1. Press the Measurement selection key.
  2. Select the Block Error Ratio measurement.
  3. Select Block Error Setup ( F1 ) and set the measurement parameters as needed.
  4. Establish an RB Test Mode connection between the UE and test set (see How Do I Set Up a Call and Make a Connection? ).
  5. If Trigger Arm is set to Single , you must press the START SINGLE key to begin the measurement.
       
    NOTE

    The time for the measurement to complete increases linearly with the Number of Blocks to Test . For example, to test 500 blocks while on a 12.2k RMC takes approximately 10 seconds (500 blocks x 20 ms/block = 10 seconds). A measurement result is not displayed until the Number of Blocks to Test has been tested. If you are testing more than 500 blocks, the block counter increments every 500 blocks to indicate measurement progress.


       

  6. Adjust Cell Power ( F7 ), AWGN Power ( F4 ), Soft Handover ( F3 ) and Cell 2 Power ( F2 ) as desired.

An example measurement result is shown below:

For an example of performing BLER measurements while on a faded channel, refer to the:

E5515C Fading Solution Application Guide

It can be downloaded at http://cp.literature.keysight.com/litweb/pdf/1000-1894.pdf .

Related Topics


Block Error Ratio (BLER) Measurement Description

Block Error Ratio Troubleshooting

Programming a Block Error Ratio Measurement