UE Information

 Last updated: April 27, 2013

 When the UE registers with the test set (see Performing a Location Update (CS Domain Registration) ), the following information is reported by the UE. You can query this information via GPIB commands, or view it on the Call Setup Screen under UE Information .

 

 IMSI

 International Mobile Subscriber Identity (used by the network to page the UE). See Test Set-Originated Connection .

 GPIB command: CALL:MS:REPorted:IMSI[:SELected]?

 

 IMEI

 International Mobile Equipment Identity.

 GPIB command: CALL:MS:REPorted:IMEI[:SELected]?

 

 Power Class

 The UE's power class defines its nominal maximum output power (see 3GPP TS 25.101 6.2).

 GPIB command: CALL:MS:REPorted:PCLass[:SELected]?

Enhanced CELL_FACH Config

This setting sets the current configuration of enhanced CELL_FACH.

GPIB command: CALL:STATus:EFACh:CONFigure?

 

HS-DSCH Reception

The HS-DSCH Reception indicates what the UE reported to the test set about its support of HS-DSCH reception in CELL_FACH. The UE uses the IE HS-PDSCH in CELL_FACH sent in the UE radio access capability comp 2 message.

GPIB command:  CALL:HSDPa:MS:REPorted:HSDSchannel:FACH?

HS-DSCH DRX

The HS-DSCH DRX indicates what the UE reported to the test set about its support of HS-DSCH DRX operation. The UE uses the IE Support of HS-DSCH DRX operation sent in the Physical channel capability message.

GPIB command:  CALL:HSDPa:MS:REPorted:HSDSchannel:DRX?

Common E-DCH

The Common E-DCH indicates what the UE has reported to the test set about its support of Common E-DCH. The UE uses the IE Support of common E-DCH sent in the UE radio access capability message.

If UE reports that it supports Common E-DCH, it implicitly indicates the support of MAC-i/is.

GPIB command: CALL:HSUPa:MS:REPorted:CEDChannel?

MAC-i/is

The MAC-i/is indicates what the UE has reported to the test set about its support of MACi/is. The UE uses the IE Support of MAC-i/is sent in the UE radio access capability message.

 GPIB command: CALL:HSUPa:MS:REPorted:IISPeed?

 Detected PRACH Signature

 This feature is only applicable to the lab application.

 When the UE sends a PRACH preamble, it uses one of the PRACH signatures that the test set has specified using the PRACH Signature parameter. If the test set has specified that more than one PRACH signature is available to the UE, in a series of PRACH bursts, the UE will randomly select which PRACH signature to use for any given burst.

 The Detected PRACH Signature result is an integer representing the PRACH signature used by the UE on its final PRACH burst (the one that the test set responded to). If the PRACH Signature setting specifies a single PRACH signature, then Detected PRACH Signature and PRACH Signature should be the same.

 For the lab application only, the PRACH preamble analysis measurement also reports the signature used by the UE for the PRACH burst it has analyzed (see PRACH Preamble Analysis Measurement Description ). If the PRACH Signature setting specifies a single PRACH signature, then the PRACH signature reported by the measurement, Detected PRACH Signature and PRACH Signature should be the same.

 GPIB command: CALL:MS:REPorted:PRAChannel:SIGnature? .

 

 Called Party Number

 This feature is only applicable to the lab application.

 This is the number the user dialed into the UE when a UE-originated call was established with the test set. If the user dialed 911, 112 or 999, the string "Emergency Call" is displayed.

 See Calling Party Number Parameters for related information.

 GPIB command: CALL:MS:REPorted:ONUMber<[:SELected]|WCDMa>?

 

 Clear UE Info

 To clear the UE reported information and counters, select Clear UE Info ( F6 ) from the Call Setup screen, or send the CALL:MS:REPorted:CLEar[:ALL]<[:SELected]|:WCDMa> command.

 

 UE Reported DB DC-HSDPA Cap

 This feature is only applicable to the lab application.

 UE reported its supporting DB-DC-HSDPA configurations.

 As seen from the table below, the first three configurations are defined in 3GPP Release 9 and the last two configurations are defined in 3GPP Release 10.

 3GPP TS 25.101 Table 5.0AA DB DC-HSDPA configurations

 DB-DC-HSDPA Configuration

 UL Band

 DL Band

 Supported in Release

 1

 I or VIII

 I and VIII

 Release 9

 2

II or IV

 II and IV

 Release 9

 3

 I or V

 I and V

 Release 9

 4

 I or XI

 I and XI

 Release 10

 5

 II or V

 II and V

 Release 10

 GPIB command: CALL:MS:REPorted:CAPability:DCHSdpa:DBANd?

 

Related Topics


 

Establishing a Connection with the UE

 HSDPA Information

 HSUPA Information and HSUPA Happy Bit Information

 Active Cell Operating Mode