PRACH Transmit On/Off Power Measurement Description

PRACH Transmit On/Off Power Measurement Description

Last updated: January 16, 2009

How is a PRACH Transmit On/Off Power Measurement Made?

Before initiating a PRACH transmit on/off measurement, turn the UE on and wait for it to camp to the test set's signal. When the PRACH transmit on/off power measurement is initiated, the test set sets Call Limit State to On to prevent successful call connection, then pages the UE. This forces the UE to transmit PRACH preamble bursts.

The test set then measures the "on" power of the first PRACH preamble burst from the UE. The test set measures the average power (without an RRC filter present) from 25 µs after the start of the PRACH access slot, to 25 µs before the end of the PRACH preamble burst (see Burst On Power Measurement Interval ).

Burst On Power Measurement Interval

The test set then measures the "off" power before and after a subsequent PRACH preamble burst ("Pre Burst Off Power" and "Post Burst Off Power," respectively). The test set measures the average power with an RRC filter in place (Root-Raised Cosine filter response with a roll off of alpha = 0.22 and a bandwidth equal to the chip rate). The Pre Burst Off Power is measured from 642 µs before the start of the PRACH access slot to 25 µs before the start of the PRACH access slot. Depending upon your test set's hardware configuration (see www.keysight.com/find/8960upgrades), the Post Burst Off Power is measured from either 25 µs or 100 µs after the end of the PRACH preamble burst to 642 µs after the end of the PRACH preamble burst. See Burst Off Power Measurement Intervals .

Burst Off Power Measurement Intervals

The PRACH transmit on/off power measurement is triggered by a combination of RF rise and protocol. The test set must first receive an RF rise which is at least -45 dBm, and which is no more than 9 dB below the expected power ( Initial PRACH TX Power if Power Control is set to Auto, or Manual Power if Power Control is set to Manual; see Receiver Control ). The test set then uses this RF rise to determine in which PRACH access slot the PRACH preamble burst is contained. The protocol trigger then triggers the measurement on that access slot.

Measurement Behavior

The UE must be camped to the test set and in idle mode before performing the PRACH Transmit On/Off Power measurement.

To perform the PRACH transmit on/off power measurement, you must set Available Subchannels (Bit Mask) to only allow one available subchannel.

You must also set PRACH Preambles to at least 3 before initiating this measurement. It is recommended that you set PRACH Preambles to 4 , PRACH Ramping Cycles (MMAX) to 1 , and Call Limit State to Off before initiating this measurement to minimize issues after the measurement has completed. See the following:

No other measurements can be running when a PRACH transmit on/off power measurement is performed. If any measurements are running when a PRACH transmit on/off power measurement is initiated, they are closed and a message is displayed to indicate that they were closed.

Other Considerations

To change the UE's Initial PRACH TX Power level (which is reported by the Burst On Power result), you can change Primary CPICH TX Power , Uplink Interference , Constant Value , Cell Power and/or CPICH RSCP (Received Signal Code Power) . If you change Primary CPICH TX Power , Uplink Interference , or Constant Value , you must force the UE to re-read the BCCH before initiating the measurement (so that it will use the same values for these settings as the test set when calculating the power of its initial PRACH preamble). If your UE supports the Broadcast Channel (BCCH) Update Procedure (SIB Contents) , set BCCH Update Page to Auto to force the UE to re-read the BCCH. If your UE does not support the BCCH Update procedure, see BCCH Update Page for suggestions on forcing the UE to re-read the BCCH.

PRACH Transmit On/Off Power Measurement Parameters

PRACH Transmit On/Off Power Measurement Results

Key 3GPP Tests Performed Using the PRACH Transmit On/Off Power Measurement

The "on" power measurement tests the open loop power control of the UE (3GPP TS 34.121, 5.4.1), while the "off" power measurement tests for unnecessary system signal leakage power (3GPP TS 34.121, 5.5). This measurement measures both the "on" power of the first PRACH preamble burst and the "off" power immediately prior to and just following any given PRACH preamble. It meets the requirements defined in 3GPP TS 34.121, section 5.5, Transmit ON/OFF Power and section 5.4.1, Open Loop Power Control in the Uplink . In order to prevent false "off" power measurements in the case where a compliant UE transmits power up to the limit of the +25 µs transient period, the start of the "off" power measurement period is delayed slightly to allow for recovery from receiver re-ranging.

Input Signal Requirements

Measurement Calibration

This measurement should be calibrated using the Calibrate Measurements function ( CALibration:MEASurements? ) when the temperature has changed by more than ± 10° C since the last calibration. If this situation exists, the integrity indicator value becomes 19 and a message is displayed indicating "Uncalibrated Due to Temperature".

Related Topics