The trigger
can be set for the following style of trigger signals. Specify a rising (positive) or falling (negative) slope.For information on triggering for specific measurement hardware, see Available Measurement Hardware for a link to your specific hardware.
This trigger parameter is shared by measurements that share the same Analyzer Configuration. Changing this parameter for one shared measurement will change it for the other shared measurements.
Trigger parameters (including this one) affect the outcome of the time record capture from hardware when creating a recording as well as when making a measurement.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |