Changes the state of the triggering system from "idle" to "wait-for-trigger", and clears the previous set of measurements from reading memory. Measurements begin when the specified trigger conditions are satisfied following the receipt of INITiate.
Parameter | Typical Return |
---|---|
(none) | (none) |
Return five DC voltage measurements, using a software trigger to start the measurements: CONF:VOLT:DC 10,0.003 |