Reads and erases all measurements from reading memory up to the specified <max_readings>. The measurements are read and erased from the reading memory starting with the oldest measurement first.
Parameter | Typical Return |
---|---|
1 to 2,000,000 (readings) Default is all readings in memory. |
(none) |
Read and remove the three oldest readings: Typical Response: #247-4.98748741E-01,-4.35163427E-01,-7.41859188E-01 The "#2" means that the next 2 digits indicate how many characters are in the returned memory string. These two digits are the "47" after the "#2". Therefore, the remainder of the string is 47 digits long: -4.98748741E-01,-4.35163427E-01,-7.41859188E-01 |
No error is generated if the reading memory contains less readings than requested. In this case, all available readings in memory are read and deleted.